Part Number: DP83867CR
The following problems have occurred in the board under development using DP83867CRRGZT.
There is no setting from MDIO, and it is launched only by Strap Configuration.
The settings related to 1000BASE-T in the Strap Configuration are as follows.
-RX_DV/RX_CTRL:Mode3(Autonego Enable)
-LED1:Mode1(advertise ability of 10/100/1000)
Case 1
With 1000Mbps Autonegotiation Enable, it links with the terminal (PC) but not with the HUB.
When the Master/Slave setting was changed to fixed Master, it linked with PC/HUB.
On the other hand, if you fixed it to Slave, it will not link to either HUB/PC.
Case 2
If set to 1000Mpbs Full-Duplex fixed, neither PC nor HUB will be linked.
Case 3
When connecting to a HUB/PC with 100M Autonego setting, the HUB/PC repeats Link Up/Down.
At that time, DP83867CR is not always linked.