Part Number: TLK2711-SP
Good Morning,
I have seen the following behaviour working with the TLK2711-SP.
I am sending two /K28.5/D5.6/ (0xC5BC) with KMSB= '0' and KLSB = '1' in a row to perform the data alignment. From time to time (every 2-3 seconds) I am receiving just one comma (1 cycle of RX_clock) and then I am receiving the expected data but repeated. As an example:
Sended: /K28.5/D5.6/K28.5/D5.6/D0.0/D0.1/...
Received: /K28.5/D5.6/D0.0/D0.0/D0.1/...
My WER (Word error rate) is in the order of 10exp(-9)
Is that an expected behaviour of TLK2711? Is it produced by some kind of elastic buffer within the TLK? By the way, I am using a Engineering model part.
Thank you and Best Regards,
Germán Coronado