Part Number: DP83867IRPAP-EVM
Other Parts Discussed in Thread: AM3358
Hi,
I want to use the DP83867IRPAP RGMII interface with AM3358's RGMII interface. I wish the RGMII interface should be configured like the following after I design the strap pins:
1. RGMII interface should be enabled after power on, so I think the Pin50(RX_D6) should be strapped as the mode 4
2. the "auto negotiation" of this RGMII interface should be enabled after power on, so I think the Pin53(RX_DV/RX_CTRL) should be strapped as mode 3
but I checked the EVM reference design schematics, they strapped the Pin50 as the mode2, and the Pin53 as mode1(open , open)
could you help me to make sure the Pin50 and Pin53 strap configuration?
thanks,
Li