Part Number: DS90UB953A-Q1
Hello,
Our customer's application is HOST->954---953->MIPI 2LANE SENSOR307. The IDx,MODE pin of DS90UB954 is pulled low by 10K resistor, and IDx of DS90UB953 is pulled low by 40.2Kohm resistor. The registers are configured as following:
TI954Q_WRITE_ID:0x60
TI953Q_WRITE_ID:0x30
//Set up Port0
WriteReg(TI954Q_WRITE_ID, 0x4C, 0x01);
//Set up Back Channel Config (0x58)
WriteReg(TI954Q_WRITE_ID,0x58,0x5E);
//Set up SER ID
WriteReg(TI954Q_WRITE_ID,0x5B,0x30);
//Set up SER Alias ID
WriteReg(TI954Q_WRITE_ID,0x5C,0x30);
//Set up Slave/Camera ID
WriteReg(TI954Q_WRITE_ID,0x5D,0x34);
//Set up Slave/Camera Alias ID
WriteReg(TI954Q_WRITE_ID,0x65,0x34);
//Set serializer CSI-2 data input from imager lane to 4 lane, 1.8V VDDIO
WriteReg(TI953Q_WRITE_ID,0x02, 0x33);
//Set GPIO1 and GPIO0 to outputs, where GPIO0 = FSYNC trigger and GPIO1 = IMX390 reset
WriteReg(TI953Q_WRITE_ID,0x0E,0x30);
//Set GPIO1 and GPIO0 to low - confirm snesor is power down mode
WriteReg(TI953Q_WRITE_ID,0x0D,0x00);//0x90
Delay_DelayMs(1);
//Bring GPIO1 high again to prepare sensor for initialization
WriteReg(TI953Q_WRITE_ID,0x0D,0x02);
//enable CSI output and CSI continuous clock, 2lane
WriteReg(TI954Q_WRITE_ID, 0x33, 0x23);
//enable CSI replicate mode
WriteReg(TI954Q_WRITE_ID, 0x21, 0x81);
//enable RX 0 port forwarding to CSI ports
WriteReg(TI954Q_WRITE_ID, 0x20, 0x20);
Now the question is that, the I2C appear error as this:
ERR:TI_I2C_Transmit() fail to send data, w_addr 0x30, r_addr 0x2, data 0x33, sts 2
ERR:TI_I2C_Transmit() fail to send data, w_addr 0x30, r_addr 0xE, data 0x30, sts 2
ERR:TI_I2C_Transmit() fail to send data, w_addr 0x30, r_addr 0xD, data 0x0, sts 2
ERR:TI_I2C_Transmit() fail to send data, w_addr 0x30, r_addr 0xD, data 0x2, sts 2
TI w_addr 0x60 Reg addr 0x00, data 0x60
TI w_addr 0x60 Reg addr 0x4C, data 0x01
TI w_addr 0x60 Reg addr 0x58, data 0x5E
TI w_addr 0x60 Reg addr 0x5B, data 0x00
TI w_addr 0x60 Reg addr 0x5C, data 0x30
TI w_addr 0x60 Reg addr 0x5D, data 0x34
TI w_addr 0x60 Reg addr 0x65, data 0x34
TI w_addr 0x30 Reg addr 0x02, data 0x30
TI w_addr 0x30 Reg addr 0x0E, data 0x30
TI w_addr 0x30 Reg addr 0x0D, data 0x30
TI w_addr 0x60 Reg addr 0x33, data 0x23
TI w_addr 0x60 Reg addr 0x21, data 0x81
TI w_addr 0x60 Reg addr 0x20, data 0x20
--------------------------------end---------------------------
Could you please help to analyze ?
Best regards
Kailyn