This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83867IS: MDIO can not work

Part Number: DP83867IS

Hi 

After power up, the pin of MDIO is always 0V. When SOC write some datas to PHY, the hign level of MDIO is 1V, can not reach the normal level 1.8V (VDDIO is 1.8V)

Disconnect the R431, the MDIO of PHY to GND is near 1M Ohm when power down and is roughly 60~70 Ohm when power up. I guess the MDIO of PHY is OD output? What's keeping it going to output low level (0V)?

SCH _ 39 Ethernet1 RGMII RJ45.pdf

thanks