Part Number: DS90UB960-Q1
Hi team
We use 960 + 953 + 1080P camera, And we use the External FrameSync Control by sending in a square waveform, the frequency of the square waveform is 30Hz, and the duty cycle is 50%, the external signal can be transfor to 953 and been output through the GPIO0 of 953. On the pin of 953 GPIO0,The signal can be measured through an oscilloscope.We can get video stream by gst command, But the stream is also abnormal, As show in the video. I turn round the camera body's angle, 0, 90, 270, 360 degree,No matter which angle, the top of the screen is always abnormal. I only connected one camera, Before I still think this is a proble of bandwidth, while I change the square waveform frequency to 1.8Hz, the problem is alse exist. Now i think this is not a problem of bandwidth, And I had configure the CSI-2 Output Lane Speed to 1.6Gbps.What's the problem?