This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB954-Q1: Is RX_FREQ the same as FPD3_MODE frequency?

Part Number: DS90UB954-Q1

Hello expert,

We are trying to dump some register value from TI-954 and found one issue below:

  •  PORT_CONFIG Register(Address 0x6D)

We configure “PORT_CONFIG Register” as “0x7e”. 

So, “FPD3_MODE” should be “10: RAW12 Mode / 75 MHz”.

 But, we read the following 2 Register:

  • RX_FREQ_HIGH (Address 0x4F) = 0x25 (37)
  • RX_FREQ_LOW (Address 0x50) = 0x00

We have no idea whether the value of “RX_FREQ” should be the same with “FPD3_MODE (i.e. 75MHz)” ? Could you help us to verify ? Many thanks.

Best regards,

Ann Lien