Part Number: SN65DPHY440SS
Hi Sir,
My customer would like design SN65DPHY440SS to enhance mage sensor MIPI signal after a long FPC.
There are 2 questions about SN65DPHY440SS. Please provide your comments.
1. The image sensor interface is CSI-2, can we swap the lane to make the layout smooth? ex: connect sensor lane0 to SN65DPHY440SS DA1, lane2 to DA0.
Customer saw the LP mode at datasheet 7.4.2, but it is for DSI, so customer want to confirm that SN65DPHY440SS can swap lanes when the sensor interface is CSI-2.
2. About I2C, customer saw the description in section 7.5: "Access to the CSR registers is supported during ultra-low power state (ULPS)", but according to 7.4.3, ULPS mode can only be entered from LP Mode.
Does it mean that the design can't use I2C when we use CSI interface?
BR,
SHH