Part Number: TPS65987DDJ
Hi everyone
I am creating new project with TPS65987DDJ. I finded table with Device Default Configurations. But I didn't find Default Configurations of GPIO pins. I need to use one GPIO pin like control signal of MUX SuperSpeed lines. And one more like Enable signal of external DC/DCs when power source is greate than 5V@900mA. My device is UFP (sink). I want to use Configuration 3 (Table 7. Device Default Configurations P.41 of DataSheet) and BP_NoWait config.
What GPIO can I use like "Port 0 Cable Orientation Event" by default (without external flash memory)?
What GPIO can I use like "Ice Lake High Current Contract Active Event" by default (without external flash memory)?
Thanks