Part Number: BQ24392
Other Parts Discussed in Thread: BQ25790, BQ25792, , BQ25150
Hi TI Team,
I need quick support for designing battery charger with below requirements.
- Capable to charging from main supply.
- Charge minimum 1 Li-Ion battery of cell capacity 250 mAH.
- Capability to charge 4 battery modules.
- Efficiency 80% minimum.
- Charging status indication through LED.
- Over voltage and over temperature protection.
- Charger should support power mains plug to support countries world-wide.
- Control over I2C bus.
- Once connected to PC USB port it should be properly detected with configurable device name.
- Should be capable of charging from adaptor as well as USB port.
The main components planning to use are listed below.
1. Battery Charger.- BQ25790 / BQ25792
2. Charger detection IC. - BQ24392
3. Microcontroller to control the Battery charger.- To control battery charger over the I2C bus.
Can you suggest suitable microcontroller which supports above requirements.?
Planning to go with a microcontroller having I2C interface and GPIO.
Is there any USB interface required for microcontroller ?
Expecting your immediate reply.
Thanks & Regards,
Siburaj