Part Number: SN65HVD234-Q1
Dear all,
I need to connect 2 devices with canbus interface.
I have no ground reference. There are available only the CanH, CanL and Power+ pins.
How can I connect them in order to exchange can messages?
The positive pin of the first device is at 42 Vdc from its internal ground.
The positive pin of the second device is at 30 Vdc from its internal ground.
Can I connect the positive line and choose a canbus driver +/-15V common mode tollerant?
Any your help is very appreciated. Best regards.
Devis