This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83822H: VDDIO of 2.5v with AVD of 1.8V

Part Number: DP83822H


Hi,

Is it possible to use the part with VDDIO = 2.5 and AVD=1.8?

Although at section 10 it is noted that any combination between VDDIO = {3.3,2.5,1.8} and AVD = {3.3,1.8} is possible, table 145 doesn't offer any condition with the use of 2.5V I\O.

Thanks,

Eran