Part Number: SN65C1168E
Can you comment on the output impedance of the drivers for SN65C1168E?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN65C1168E
Can you comment on the output impedance of the drivers for SN65C1168E?
Gregory,
What do you want to know about the output impedance? The impedance varies with the load condition. For example, assume SN65C1168E generates 3V on 100Ohm load with 5V supply. The output current drawn from the driver is 30mA. The driver's impedance is around 33Ohm in this case.
Regards,
Hao