Part Number: DP83822IF
Hello,
We are using the DP83822IF in 100BASE-FX mode. In the datasheet it is recommended to use the LED_1/GPIO (pin 24) in Signal Detect mode when in FX mode. However we also would like to control an LED with this pin. Is it possible to use both Signal Detect and control an LED using this pin? If not what is the recommended approach?
In connection with this, if we do not use the LED_1 in Signal Detect mode how is the Fiber link-up/down detected?
Thanks.