This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MIPI(or Parallel) to LVDS (Serializer)



Hi Expert,

I have a new project that needs camera with a long cable.

The camera sensor has dual interfaces that are MIPI and parallel and CPU(QCS610) has only MIPI CSI.

Could you recommend the interface convert IC for as below:

Camera seneor (MIPI/Parallel) -> LVDS(Serializer) -> LVDS(deserializer) -> MIPI

Thanks in advance,

Devin

  • Hello Devin, 

    Could you give a little more information regarding the camera resolution/bandwidth? I could suggest that you use a DS90UB953/933 (SER) and a DS90UB954 (DES). The DS90UB953 has a CSI-2 interface and can handle larger camera resolutions. The DS90UB933 has a parallel interface and can handle smaller camera resolutions. The DS90UB954 will output CSI-2 data. 

    Thanks, 
    Sally