Part Number: DP83848K
Hello,
I'd like to ask a question about DP83848K Auto-neg and auto-mdix enable register setting at fixed 100M advertised speed.
If set the register 0x4 as following value, is it working as '100M Full Duplex and Half Duplex auto nego mode'?
According to datasheet, it looks not possible to set advertisement only at '100M Full Duplex mode'. is it right?
TX_FD : 1
TX : 1
10_FD : 0
10 : 0
Table 6-13. Auto-Negotiation Advertisement Register (ANAR), address 0x04 (continued)
Thanks and Best Regards.
Jerome Shin