Part Number: TPD4E05U06DQAEVM
Other Parts Discussed in Thread: TPD4E05U06
In point 10.2.1 of https://www.ti.com/lit/ds/symlink/tpd4e05u06.pdf (page 24) Figure 24 shows layout example for HDMi routing when parallel paths are connected to NC pads of the device. I am working on Ethernet traces however this should not matter. Is it allowed to connect parallel paths to NC pads of the ESD device? On Page 4 the description for NC is the following: "Not connected; Used for optional straight-through routing. Can be left floating or grounded". So it looks like it is ok, however i am not too sure. Would this cause some problems with data flow? Cheers.