Part Number: SN65DSI84-Q1
Hi team,
Can you answer the following questions?
-. SN65DSI84-Q1(D-PHY1.0) is backward ompatible with D-PHY1.2 version in SoC?
-. Below is the vidoe format for two streams. Can SN65DSI84-Q1 support the spec with the D-PHY 1.2 TX of SoC?
Video output : overhead 35%, Blank Interval: 1.35
1. 1920x720x60Hz / 24bpp => 2.687Gbps (w/ overhead)
2. 800x480x60Hx / 24bpp => 0.746Gbps (w/ overhead)
=> Total 3.434Gbps
Thanks,
Sam Lee