This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB941AS-Q1: How to configure 941 and 928 for HV mode display?

Part Number: DS90UB941AS-Q1


Hi team,

As shown in the block diagram below,
1. When the 941-928-DE Mode screen is on, the screen can work normally at this time, and the register export is shown below. (OK.txt)
2. When the 941-928HV Mode screen is on, the screen cannot work normally at this time, and the register export is shown below. (NG.txt)
3. When I83-927-928 HVMode screen, the screen can work normally at this time.
From the above several tests, it seems that the HV mode screen needs to be configured accordingly when used with the HV mode screen. Any suggestions are appreciated.

/cfs-file/__key/communityserver-discussions-components-files/138/OK.txt

/cfs-file/__key/communityserver-discussions-components-files/138/NG.txt

Best regards,

Yu