Part Number: DS90UB962-Q1
Module configuration: ISP output: 1920x384, 50FPS, DVP output, YUV422.
Debugging SerDes (DS90UB933+DS90UB962), sometimes lighting and sometimes not lighting phenomenon.
There is a problem locating DS90UB962 Line_Count, Line_Len(0x73, 0x74, 0x75, 0x76) for transmission, I wonder what caused it?
SerDes initializes setting:
0x60, 0x01, 0x12, 1,1000,
0x60, 0x4C, 0x01, 1,
0x60, 0x70, 0x1F, 1,
0x60, 0x6D, 0x7F, 1,
0x60, 0x6E, 0xAA, 1,
0x60, 0x4c, 0x0f, 1,
0x60, 0x5C, 0x18, 1,
0x60, 0x7C, 0x81, 1,
0x60, 0x10, 0x91, 1, 100,
0x60, 0x58, 0x58, 1,
0x18, 0x0D, 0x99,1,
0x60, 0x19, 0x0D, 1,
0x60, 0x1A, 0x04, 1,
0x60, 0x1B, 0x75, 1,
0x60, 0x1C, 0x2E, 1,
0x60, 0x18, 0x01, 1,
0x60, 0x20, 0x00, 1,
0x60, 0x32, 0x01, 1,
0x60, 0x33, 0x01, 1,