Part Number: TPS65987D
Hello,
We want to program the flash memory for TPS65987D from a connector and use external 3.3V from the connector to power it , then , when the flash is programmed , power it from LDO_3V3 as recommended.
The TPS65987D is in dead battery mode "BP_NoWait". So after we connect the USB-C cable it can read the flash and load the configs.
My question is, how to connect the external 3.3V from connector , to power the flash memory?
Should the connection be : external 3.3V to LDO_3V3 that is connected to flash memory , or external 3.3V to VIN_3V3 pin that's gonna supply the power to LDO_3V3 and connect the flash memory to LDO_3V3?
Thanks in advance,
Eriks