Part Number: TCA9406
Hello!
Do you have a maximum operating junction temperature for this device? I do not have estimated power dissipation values for this part yet, and want to set my upper limit based on your direction.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TCA9406
Hello!
Do you have a maximum operating junction temperature for this device? I do not have estimated power dissipation values for this part yet, and want to set my upper limit based on your direction.
Hey Martin,
I2C translators are typically low power devices so there shouldn't be much dissipation across them. Generally we the recommended max junction temperature is +5C of the max recommended ambient so in this case it would be 85C+5C = 90C.
For an absolute maximum junction temperature. I was able to find simulation data which showed the part was atleast tested at 100C. Looking at another device sharing almost the exact same internal IP (in terms of die), I was able to find that the 'twin brother' of this device has an absolute max junction spec'd at 150C... I can't guarantee the bond wires/leadframe are the same but the dies themselves are comparable and this would suggest 150C may be the absolute max junction.
-Bobby