Part Number: THVD1451
Other Parts Discussed in Thread: SN65HVD01
Hello,
Does TI have any full duplex RS485 transceivers that can operate at 1.8V?
Thanks,
Adam
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Adam,
At the moment, unfortunately not. We have the half-duplex SN65HVD01 device which can support a 1.8-V IO voltage rail. Two of those devices could be used if the application were full-duplex rather than half-duplex. Alternatively, a full-duplex device supporting higher voltages like THVD1451 could be paired with a level-shifter device.
Regards,
Max
Thanks Max. For the THVD1451 does it hold the bus in '0' when not powered or does it behave as high-z?
Best,
Adam
Hi Adam,
The bus lines will be high-Z when the THVD1451 transceiver is unpowered so that communication among other, powered nodes is not disturbed.
Regards,
Max