Part Number: DP83869HM
Other Parts Discussed in Thread: DP83869
Hi,
Would like to know if there are any standard SFP module list available that are tested/evaluated with DP83869 in the Optical to RGMII mode for 1Gbps operation.
Regards,
Sudarshan
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Sudarshan,
We don't have a recommended list of SFP modules. Let me check and get back about the SFPs we have used frequently in lab.
--
Regards,
Vikram
Hi Vikarm,
Thanks.
We are using DP83869 in Fibre to RGMII Mode of operation.
Regards,
Sudarshan
Hi Sudarshan,
I got the following list of SFPs that we have seen being used at end applications :
1. Cisco GLC-FE-100Fx
2. Avago HFBR 57E0APZ
--
Regards,
Vikram
Hi Vikram,
Thank you very much for the feedback. Both are 100-Fx based modules.
I hope DP83869 also support 100base-x as well. Please let us know if any modules were tested in this speed grade also.
Regards,
Sudarshan
Hi Sudarshan,
For 1000BFx I have received following list from field. These SFPs have been used during tests with 869 evaluation boards as link-partners.
1. IPOLEX ASF85-24-X2
2. INTELLINET 545006
3. UBIQUITI UF-MM-1G
4. INTELLINET 506724
5. OPTCORE OSP125-3110DCR
Hope it helps.
--
Regards,
Vikram