Part Number: P82B96
Hello,
From the datasheet, higher voltage of +V cable can be used for longer cable, right?
Could you tell me how to determine the +V cable voltage?
Best regards,
Katsu
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: P82B96
Hello,
From the datasheet, higher voltage of +V cable can be used for longer cable, right?
Could you tell me how to determine the +V cable voltage?
Best regards,
Katsu
Hello Katsu-san,
The absolute max voltage we allow on the Vcc is 18V and the recommended max is 15V.
Using a higher Vcc allows for larger noise margins on the Rx/Ry lines. (refer to the Vit for Rx/Ry in the electrical characteristics)
If you are not expecting noise to be an issue on the cable end, then using a lower Vcc level can be acceptable though if you expect noise to be a potential concern then choosing the largest Vcc value would be in your best interest. (We don't have a set rule on what the +V voltage needs to be but larger provides better noise protection on the cable side).
The Sx/Sy lines can be pulled up to a different logic level than the Vcc of the device.
Let me know if you have additional questions or if something I explained is unclear.
Thanks,
-Bobby