Part Number: SN65LVCP22
Hello.
Let me ask you some questions about the SN65LVCP22.
1. Does SN65LVCP22 have a built-in FAIL SAFE function?
Looking at the circuit principle diagram, it does not seem to have the FAIL SAFE function.
2. I think you will add pull-ups and pull-downs to the inputs when inserting an open fail. At that time, does the pulse duty specification deviate from the data sheet?
If a general offset within 100 mV is added, will it not meet the specifications?
3. In order to avoid the effect of 2. , if an open fail is not added to the input circuit with only the terminating resistor, an undefined state may occur internally.
I am trying to select with the SEL signal to the side that is always connected. Is there a problem?
Thank you for your cooperation.