Part Number: DS90UH948-Q1
Hi
Can I2C from DS90UH947 side control DS90UH948 when 948 pattern gen are enabled ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UH948-Q1
Hi
Can I2C from DS90UH947 side control DS90UH948 when 948 pattern gen are enabled ?
Hello PYTsai,
It depends on the clocking mode selected for the pattern generator. If the internal deserializer clock is selected for the patgen clock source, then the bidirectional control channel will not be functional while the test is running. However if you use the external clock (clock from the serializer forward channel) as the pattern clock source then the bidirectional control channel will continue to function during the test.
Best Regards,
Casey