Part Number: TPS65982
Hi,
I have enabled all bits in register 0x14 (IntMask1) via application firmware and am seeing IRQs for e.g. VDMReceived (bit 11 in bytes 1-4), StatusUpdate (bit 26 in byte 1-4) or Error_ProtocolError (bit 6 in bytes 5-8) but i'm never seeing any IRQs for VDMmsgSent sent (bit 18 in bytes 5-8) or VDMEnteredMode (bit 17 in bytes 5-8).
- Are there other prerequisites to enable IRQs for these events?
- Are any IRQs dependent on whether mode auto entry is enabled?