Other Parts Discussed in Thread: CSD13380F3
Hi. I have an application where I think I need a P-Channel Depletion mode MOSFET to switch a low current and low voltage. Basically the configuration is: with no Gate voltage (either floating or 0v), I need to switch +2.5v - +5.1v through to the Drain from the Source. The Drain will be attached to ground through a 2K resistor and then to a high impedance input pin. The Source will be attached to a voltage that can be from ~ +2.5v to +5.1v. The gate voltage will be digital: either 1.8v and 0v -or- it will be 3.3v and 0v. Does TI make anything that will work for this application? Is a P-Channel Depletion mode the right kind for this application where I need it to normally be conducting even when the Gate is open? Thank You.