Part Number: TIR1000
Hello experts,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TIR1000
Hello experts,
Hello Akashi-san,
The 16X clock input can be at most 2 MHz. The degree of allowable frequency variation between the local clock and the serial baud rate is not characterized for this device since it is more of a system-level concern related to the UART data strobing. At the decoder level, frequency mismatches or jitter could result in short-term misinterpretations of the serial bit value. An example of this is shown in Figure 6 of the datasheet. Typically if the UART samples at the center of the expected bit period these short-duration glitches can be tolerated.
Regards,
Max
Hello Max-san,
That is correct. The nominal output rise/fall times are specified in the Switching Characteristics table, but there is no restriction defined for the input rise/fall times.
Max