Part Number: THVD1451
Hi all,
I’d like to know if THVD1451/1452 meet the CC-LINK certification.
It is not specified on the datasheet, so it would be greatly appreciated if someone could tell me.
Best regards,
Kurumi Hasegawa
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: THVD1451
Hi all,
I’d like to know if THVD1451/1452 meet the CC-LINK certification.
It is not specified on the datasheet, so it would be greatly appreciated if someone could tell me.
Best regards,
Kurumi Hasegawa
Hasegawa-san,
According to the CC-Link website (http://am.cc-link.org/en/cclink/cclink/spec1.html), the physical layer is compliant to EIA-485 and the applications can operate up to 10 Mbps and with 64 nodes per network. The THVD145x devices can meet these requirements.
Regards,
Max