Part Number: HD3SS214
Other Parts Discussed in Thread: TDP142,
Dear Sirs,
My customer use TDP142 and HD3SS214 for their KVM design.
Here is the block.
They want to know,
1. if 3440x1440@120~144Hz can be support by their design?
2. If it is possible to support up to 8K resolution since after customer test, it only can support 5120x2880@60Hz.
3. Can we use all 8Gbps bandwidth? if not, what will be the reason to lower the bandwidth that can be use?
Thanks.