Part Number: SN65HVD1050
Hi team,
Could you kindly advise the Icc in the below conditions?
<Customer’s conditions>
- Node 30
- Termination 120 ohm (both end of the bus)
<Questions>
- Is the Icc of receiver node same with the Icc of recessive mode ? Only one device in the CAN bus transmit data.
- What situation is the most largest current consumption at 30 node ?
When all the devices in the CAN bus transmit ACK is largest ? or other conditions ?
Customer would like to make sure not only for IC but also total current consumption in the CAN bus.
Thank you and best regards,
Michiaki