Part Number: TUSB1310A
Hi,Staff
This is a consultation about the TUSB1310A (USB3.0 transceiver) failure.
There is a problem that USB3.0 communication is not possible.
(It is possible to communicate with USB2.0)
TUSB1310A (USB3.0 transceiver)
It has been confirmed that communication is possible by cooling with a cooling spray.
When there is a problem with the USB analyzer
Power States (See TUSB1310A Datasheet 5.3.4.1 USB Power Management)
When it cools down, it works normally.
There are some boards that can make several boards and communicate with USB3.0.
I think that the operation is unstable.
※It is not a new design.
Please tell me the points to investigate the cause.
best regards
cafain