Part Number: DS90UB954-Q1
No problem with the LOCK in the Deserializer. But 954 MIPI DATA OUTPUT is abnormal.
Could you check if there is anything wrong with the setting below?
SENSOR OUTPUT
RAW 12 BIT / PCLK 54MHz / MCLK 27MHz / 25fps
954 Setting Value(0x30)
0x0D 0xB0
0x0C 0x81
0x20 0x20
0x1F 0x02
0x4C 0x01
0x58 0x58
0x7C 0x01
0x6D 0x7E
0x4C 0x01
// I2C Alias Port0
0x5B 0xB0 // Write SER Origianl address
0x5C 0xB0 // Write SER Changing address
0x5D 0x20 // Write SENSOR Original address
0x65 0x20 // Write SENSOR Changing address
0x5E 0x14 // Write PMIC Original address
0x66 0x14 // Write PMIC Changing address
0x5F 0xA2 // Write EEPROM Original address
0x67 0xA2 // Write EEPROM Changing address
// FPD RAW12 Virtual Channel
0x4C 0x01 // FPD RX0 Port Config
0x71 0x2C // VC0 ID
0x4C 0x01 // FPD Port Config
0xbc 0xc3
sleep 20
0x6E 0x98
0x33 0x01 // MIPI CSI Port0 Enable, 4Lane
913 Setting Value(0x58)
0x05 0x1a
0x03 0xc5