Part Number: TUSB321AI
Other Parts Discussed in Thread: TUSB321, HD3SS3212
Hi.
My customer is developing cc controller using TUSB321AI and HD3SS3212IRKST.
But the following issues occurred.
1) Operates only in UFP mode
2) Normal operation when using USB type C to USB type C cable
When using a USB type C to USB type A cable, the operation differs depending on the direction of the USB type C connector.
When connecting to the USB type C top side: Recognized as USB 3.0
When connecting the USB type C bottom side: Recognized as USB 2.0
CC1, CC2, and SEL ports operate normally
I need help with this issue.
Please review the attached circuit diagram.