Part Number: SN65HVD11
Other Parts Discussed in Thread: THVD1450, THVD1410
Hello to TI interface support team ,
I use SN65HVD11QD part in connections between PCB's and in to PCB of my project , according to figure attached ( Star connection with short distances In figure 50cm to each PCB , 10cm into PCB distance ) . Can you please recommend places locate termination resistors , there is 13 units of SN65HVD11QD i use connect together.
1. Mode operation #1 : 4 units connected together in one PCB , 3 PCB connected together on parallel connetion on main PCB ( #4 on figure ) without PC .
2. Mode Operation #2 : PC connection to the system of 13 X SN65HVD11QD ( according to figure below) .
B.R
Alexander Burtakov