This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH1297: OUT0 Mute

Guru 29720 points

Part Number: LMH1297

Hi Team,

There is two way to set OUT0 Mute as the following.

1) CTLE/CDR Register 0x1E[7:5]=111
2) ConfigIO Register 0x30[7:6]=11

What is the difference between these?
My customer confirmed 1) is less power consumption than 2) when mute OUT0.

Best Regards,
Yaita

  • Hi Yaita-San,

    In case of of #1 that you have noted, there is a m,ux that selects between different signals(for example raw mode, recovered clock). In 2nd case, the logic that mutes is before the mux for case #1.

    Regards,, Nasser

  • Hi Nasser-san,

    Thank you for your reply.
    Regarding your information, it seems #2 is less power consumption than #1 however it is actually opposite.
    Do you know why #2 consume more power than #1? 

    1) CTLE/CDR Register 0x1E[7:5]=111: 122mA -> 119mA(mute)
    2) ConfigIO Register 0x30[7:6]=11: 122mA -> 122mA(mute)

    Best Regards,
    Yaita

  • Hi Yaita-San,

    In 2nd case, the logic that mutes OUT0 is BEFORE the mux that is controlled reg 0x1E. Therefor there is more buffering before the mux and therefor there is more current comsumption(~3mA).

    Regards,, Nasser