Part Number: DP83867E
Other Parts Discussed in Thread: DP83869,
Hello, I am developing a simple 10/100/1000 repeater and your DP83867 gigabit ethernet PHY has caught my eye as a potentially good solution to this problem. My goal would be to connect the 2 PHY chips with SGMII back to back. The reason for using SGMII is I would in the second phase of the project connect a simple LVDS fanout buffer to RX and TX SGMII line so I can monitor the traffic in each direction.
My questions are:
I would need a confirmation is this possible using DP83867, or maybe DP83869 is better for this job (I need the latency to be lowest possible)?
I have read that SGMII auto-negotiation can pose a problem, is it possible to overcome this problem by setting one PHY as master, and the other one as slave (it is important for me to have 10/100/1000 MDI capability)?
Regarding the traffic monitoring feature, is it possible to route outputs of the LVDS fanout buffer to another DP83867 chips so they can convert both SGMII traffic directions to MDI (this means that monitoring PHYs would be unidirectional, only RX would be connected)?
Thanks