Part Number: TUSB2077A
Hello,
I have issue with PORTPWR and PORTDIS pins. I have attached the schematic sheets related to it. I want to use LEDs on those pins for troubleshooting the product in the field. The behavior of the LEDs does not seem to respect the description in the device datasheet. More precisely:
1. D22 flash a couple of times during and stays OFF after the first short-circuit on any downstream port (any between port 1 to 6 in my case). I was expecting D22 to stay ON because at least 1 other port is powered after the short circuit. D22 is ON before first short circuit.
2. D21 stays ON even after all 6 downstream ports are disabled after short circuits. I was expecting it to turn OFF right after the first short circuit.
3. D20 and D21 flash a single time after I connect the upstream port. After that, as described in #2, D21 stays ON and D20 stays OFF. I was expecting D20 to turn ON after the first short circuit.
I have confirmed that the USB output voltages are 0 V after short circuits. Problems #1 and #2 are observed when the upstream port is connected (and detected by the computer). I have no USB communication issue using my circuit.
Have I misunderstood the device datasheet? Have you seen this behavior before?
Best regards,
ClementSupport for TI Hub.pdf