Part Number: DS90UB954-Q1
Other Parts Discussed in Thread: DS90UB933-Q1,
I am using DS90UB954-Q1 paired with DS90UB933-Q1. I am constantly getting "Packet buffer error" (RX_PORT_STS2 register). I run BIST using pixel clock from image sensor connected to DS90UB933-Q1 and I did not get any errors (I run test for several hours). CSI lane speed is set to 1.6Gbps and all 4 lanes are used. I am using RAW10 mode. I tried to modify CSI registers 0x44-0x48 but that did not help. Besides input being faster than the output (which is not the case here), what else may be causing this "Packet buffer error"?