Part Number: TPS65987D
Other Parts Discussed in Thread: TPS65987S
I am trying to use the TPS65987D in conjunction with the TUSB1046A to create a USBC DFP DP Alt mode port sink powered from the display.
Regardless of the contents of the SPI EEPROM, the TPS65987D broadcasts in PD rev3 (PD rev2 selected in NVM) and broadcasts the source capabilities that have been disabled in the config tool and then resets after about 300ms and starts the whole process over again. VBUS is coming in from the display and powering the TPS65987s, PP_HV1 is 5V, the EEPROM appears to load, there is data on the CC line, but the PD communications seem to have nothing to do with the EEPROM settings and then this ~300ms long sequence just keeps starting and stopping forever.
I have verified the NVM contents and it matches the full binary file created by the config tool. I would say the TPS65987d is ignoring the NVM, but when I remove the NVM, the TPS65987D advertises the source capabilities long then just stops.
I do not see how the forever restarting is a OC or OV issue.
Need some advise on how to proceed.