This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65987D: TPS65987 Configuration and Setup

Part Number: TPS65987D
Other Parts Discussed in Thread: TPS65987

A couple more things...

It would be nice if the TI Programming Utility didn't hard-code some of the programming loops. One of the solder connections to our FLASH chip connected to the TPS65987 wasn't making good contact and the Programming Utility just "Hung" indefinitely. A timeout loop and error message of some sort would have been very helpful.

I have a question about the ADCIN1 pin. We had it configured so that it should have configured the TPS65987 as a UFP 5V~20V in the event the FLASH didn't configure the chip. That did not happen. If the FLASH was not programmed, the TPS65987 continually reset every 750ms waiting for the FLASH. Would you explain how the ADCIN1 pin should work in a little more detail?

It looks like the FLASH chip you are using on the EVM is going end-of-life (MX25L8006EM1I-12G). Do you have a suitable replacement for this part?

Thanks for your help!

--Del