Part Number: TUSB9261
Hi team,
The customer designed a hard disk box using TUSB9261 chip, but the transmission speed is only about 190MB/s, only half of the theoretical speed, which can not reach the maximum transmission speed of 3Gbps given in the manual. The hard disk used is gen3 hard disk, and the log printed by serial port is as follows:
========================================================
|| TUSB926x Firmware v1.06 [Jan 5 2018 12:01:27] ||
|| Device ID: 0x0000 ||
========================================================
Reset Flag(s): [Power-Up]
[0000000001] Datapath RAM Usage: 80208 / 81920 bytes.
[0000000001] Supported NCQ Depth: 32
[0000000001] U1/U2 Transistions: OFF
[0000000001] USB PHY Suspend: ON
[0000000001] SATA LPM: OFF
[0000000001] Device is Self-powered.
[0000000001] -> usb_hal_init()
[0000000001] USB Core Ver: 0x120a.
[0000000001] USB SSC is OFF.
[0000000051] -> usb_hal_connect()
[0000000051][-> ahci_init()
[0000000051] -> ahci_hba_reset()
[0000000065] USB Reset event occurred.
[0000000065] LTSSM state = (0x7) POLLING.
[0000000070] Connected at SUPER speed.
[0000000070] -> usb_hal_set_address() - addr: 0xd.
[0000000177] -> handle_usb_set_configuration() - val = 1.
[0000000178] -> usb_hal_set_U1_initiate_enable() - 1.
[0000000178] -> usb_hal_set_U2_initiate_enable() - 1.
[0000000306] -> ahci_wait_complete() timed out! Rd: 0xfb000128 = 0x00000000, cmplt_val = 0x00000003.
[0000000306] -> ahci_port_reset(0)
[0000000361] -> ahci_wait_complete() timed out! Rd: 0xfb000128 = 0x00000000, cmplt_val = 0x00000003.
[0000000361] -> ahci_port_reset(0)
[0000000416] -> ahci_wait_complete() timed out! Rd: 0xfb000128 = 0x00000000, cmplt_val = 0x00000003.
[0000000416] -> ahci_port_reset(0)
[0000000426] SATA Gen-2 speed negotiated.
[0000008797]
[0000008797] ================================================
[0000008797] IDENTIFY DEVICE INFO
[0000008797] ================================================
[0000008797]
[0000008797] Model: INTEL SSDSC2KB038T8
[0000008797] FW Rev: XCV10110
[0000008797] Serial: PHYF946600QQ3P8EGN
[0000008797] TRIM Support: Yes [DRAT][RZAT]
[0000008797]
[0000008797] Spec Compliance: ATA-7
[0000008797] Removable Media: No
[0000008797] UDMA Modes = 0x407f
[0000008797] PIO Modes = 0x0003
[0000008797]
[0000008797] LBA48: Yes
[0000008797] Max LBA = 0x00000001 bf1f72b0
[0000008797] Write FUA: Yes
[0000008797] World Wide Name = 0x55cd2e41 513c90d2
[0000008797]
[0000008797] SATA Speed: Gen3
[0000008797] NCQ Support: Yes
[0000008797] Queue Depth = 31
[0000008797]
[0000008797] Logical Sector Size = 512 bytes
[0000008797] Physical Sector Size = 4096 bytes
[0000008797] Logical Sector Offset = 0
[0000008797]
[0000008797] ================================================
[0000008881] Connected to 1 AHCI device(s).
[0000008884] AHCI task file error! P0TFD error = 0x04, status = 0x51.
[0000008884] -> ums_bot_ata_error_callback() - gBOT_state = 3.
[0000008884] -> ums_bot_send_CSW() - status = FAILED. CDB[0] = 0xa2.
[0000008884] AHCI task file error! P0TFD error = 0x04, status = 0x51.
[0000008884] -> ums_bot_ata_error_callback() - gBOT_state = 3.
[0000008884] -> ums_bot_send_CSW() - status = FAILED. CDB[0] = 0xa2.
[0000008884] AHCI task file error! P0TFD error = 0x04, status = 0x51.
[0000008884] -> ums_bot_ata_error_callback() - gBOT_state = 3.
[0000008884] -> ums_bot_send_CSW() - status = FAILED. CDB[0] = 0xa2.
[0000008885] AHCI task file error! P0TFD error = 0x04, status = 0x51.
[0000008885] -> ums_bot_ata_error_callback() - gBOT_state = 3.
[0000008885] -> ums_bot_send_CSW() - status = FAILED. CDB[0] = 0xa2.
[0000008888] AHCI task file error! P0TFD error = 0x04, status = 0x51.
[0000008888] -> ums_bot_ata_error_callback() - gBOT_state = 3.
[0000008888] -> ums_bot_send_CSW() - status = FAILED. CDB[0] = 0xa2.
[0000008888] AHCI task file error! P0TFD error = 0x04, status = 0x51.
[0000008888] -> ums_bot_ata_error_callback() - gBOT_state = 3.
[0000008888] -> ums_bot_send_CSW() - status = FAILED. CDB[0] = 0xa2.
[0000008889] -> ums_bot_case_handler() - case 5.
[0000008889] -> ums_bot_case_handler() - case 5.
[0000008898] @Warning: scsi_handle_mode_sense_cmd() - page code 0x1c not supported.
[0000008898] -> ums_bot_send_CSW() - status = FAILED. CDB[0] = 0x1a.
[0000008898] -> ums_bot_case_handler() - case 5.
[0000008899] -> ums_bot_case_handler() - case 5.
[0000008899] -> ums_bot_case_handler() - case 5.
[0000008901] -> ums_bot_case_handler() - case 5.
[0000008904] -> ums_bot_case_handler() - case 5.
[0000008905] -> ums_bot_case_handler() - case 5.
[0000008917] -> ums_bot_case_handler() - case 5.
[0000008918] -> ums_bot_case_handler() - case 5.
[0000008925] -> ums_bot_case_handler() - case 5.
[0000008925] -> ums_bot_case_handler() - case 5.
[0000009809] -> ums_bot_case_handler() - case 5.
[0000009811] -> ums_bot_case_handler() - case 5.
[0000067967] LTSSM state = (0x3) U3.
[0000116504] -> usb_hal_handle_resume()
[0000116504] -> usb_hal_handle_resume()
[0000116504] LTSSM state = (0x8) RECOVERY.
[0000116508] -> ums_bot_case_handler() - case 5.
[0000116709] -> ums_bot_case_handler() - case 5.
[0000117022] -> ums_bot_case_handler() - case 5.
[0000117371] -> ums_bot_case_handler() - case 5.
[0000117679] -> ums_bot_case_handler() - case 5.
[0000118018] -> ums_bot_case_handler() - case 5.
[0000118350] -> ums_bot_case_handler() - case 5.
[0000118659] -> ums_bot_case_handler() - case 5.
[0000118967] -> ums_bot_case_handler() - case 5.
[0000119268] -> ums_bot_case_handler() - case 5.
[0000119627] -> ums_bot_case_handler() - case 5.
[0000119938] -> ums_bot_case_handler() - case 5.
[0000120265] -> ums_bot_case_handler() - case 5.
[0000120565] -> ums_bot_case_handler() - case 5.
[0000120884] -> ums_bot_case_handler() - case 5.
[0000121207] -> ums_bot_case_handler() - case 5.
[0000121505] -> ums_bot_case_handler() - case 5.
[0000121878] -> ums_bot_case_handler() - case 5.
[0000122561] -> ums_bot_case_handler() - case 5.
[0000123219] -> ums_bot_case_handler() - case 5.
[0000123880] -> ums_bot_case_handler() - case 5.
[0000124448] -> ums_bot_case_handler() - case 5.
[0000125004] -> ums_bot_case_handler() - case 5.
[0000125613] -> ums_bot_case_handler() - case 5.
[0000126242] -> ums_bot_case_handler() - case 5.
[0000126828] -> ums_bot_case_handler() - case 5.
[0000127741] -> ums_bot_case_handler() - case 5.
[0000128673] -> ums_bot_case_handler() - case 5.
[0000182463] LTSSM state = (0x3) U3.
Could you give me any suggestion?
Best Regards,
Amy Luo