Other Parts Discussed in Thread: HD3SS215, TMDS261B, TFP401A, SN65LVDS93A, DS90C387A
Hi team
I am wondering if we have the solution about HDMI to LVDS and HDMI to USB3.0?
1. HDMI to LVDS
- Requirements:
Input: 2 HDMI sources (choose one out of two)
Output: 1 channel LVDS output
I have found one possible solution through this link
https://e2e.ti.com/support/interface/f/138/t/878594?keyMatch=HDMI%20TO%20LVDS&tisearch=Search-EN-everything
2 HDMI sources ----> Mux -> RX -> TX ------> 1 LVDS output
Mux: HD3SS215(6Gbps) or TMDS261B (3Gbps)
RX: TFP401A
TX: SN65LVDS93A
However, I am not sure if this solution can meet the customer's requirements. What else detailed specs or requirements needed to be gathered from the customer?
2. HDMI to USB3.0
- Requirements:
Output: support 1080P@60, if support windows platform without the requirement of the driver, that would be great.
I didn't found related devices but have found some products with such function through google. Do we have the solution convert HDMI to USB3.0?
shawn-wang@ti.com
Thank you.