This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MAX3238E: Could we apply a RS232 level on RINx pin (RS232 line data input) when the IC is not powered (VCC=0).

Part Number: MAX3238E
Other Parts Discussed in Thread: MAX3238

Hello,

In a new project, I want to use MAX3238E IC.  In a particular situation, MAX3238E is not powered, whereas RS232 signals are present (imposed by a RS232 peripheral).

So I have 2 questions:

- Could we apply a RS232 level on RINx pin (RS232 line data input) when the MAX3238 IC is not powered (VCC=0).
- if it's allowed,  what is the input impedance of RINx pin when Vcc=0V,?

Best Regards.

Sylvain