This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83822I: DC and AC overshoot & undershoot values are missing in the datasheet for the I/O lines.

Part Number: DP83822I


Hi, 

I want to perform the Signal integrity analysis for the RGMII interface. I need to know the maximum allowed voltages for the RGMII signals. I am using VDDIO as 1.8V. In the Electrical Characteristics, for VDDIO = 1.8V, the VIH min is 1.3V but the max value is not given. What is the allowed DC and AC overshoot ? Similarly for VIL, max is 0.5V but what is the allowed DC and AC undershoot?