Part Number: SN65HVD33
Hi,
If using the chip as a RS422 driver would it be correct to assume that the differential impedance of the trace (A,B,Y,Z) to be 100 ohms?
Thank you,
HSG
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN65HVD33
Hi,
If using the chip as a RS422 driver would it be correct to assume that the differential impedance of the trace (A,B,Y,Z) to be 100 ohms?
Thank you,
HSG
HSG,
I may be misunderstanding your question, but the differential impedance of a trace would be determined by its geometry (width, distance to reference plane, etc.) and the dielectric material properties and would be independent of the transceiver used. You are right, though, that RS-422 signals are typically sent over 100-Ohm cabling and would be terminated via 100 Ohms at the further receiver. So, if SN65HVD33 were to be used in an RS-422 application it would likely see differential output loading of 100 Ohms.
Max