Part Number: TPS65987D
Other Parts Discussed in Thread: TPS65987
We would like to use TPS65987D in one of ours designs where our device is charging tablet and the tablet is host. We were able to setup evaluation kit part (P/N TPS65987EVM) to negotiate power delivery in a way that our device is charging the tablet while the application on the tablet is communicating with the device. We have working configuration (port is configured as DRP) and we are able to load (export) settings into TPS65987D memory. However, we are not able to store settings in the flash memory. We are using TPS65987EVM to conduct this test and Configuration application version 6.1.1. Can someone explain how to store configuration in FLASH memory so we do not have to reprogram the TPS65987 every time we power on our device.