Part Number: TMDS250
Other Parts Discussed in Thread: TFP401A, DS90C387A, HD3SS215, TS3DV642
Hi team
How to select an HDMI 2:1 Mux?
Specs:
- 1920×1080@60Hz
- 24 bits color
- Two inputs and one output
The bandwidth is 1.49Gbps according to the bandwidth calculator.
It seems that TMDS250 (2.5Gbps 2-TO-1 DVI/HDMI SWITCH) can meet the bandwidth requirement but the datasheet says it only supports 12 bits color depth for 1080P. What is the reason?
And I am also wondering if you could recommend a suitable mux for this application. Thank you.